8/19/2020 4:42 AM | |
Joined: 5/8/2017 Last visit: 9/30/2024 Posts: 13 Rating: (0) |
Good Day. I want to upload program from Sinamics DCM ,version A1. Used with Siemens PC Adapter USB A2 . But cannot communicate with the Sinamics DCM drive . Use window 10 and Stater software V5.3.0.1 Please advise, how to solve the problem. Thank You Satia Universal Cable (M) Berhad Malaysia [snip] ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/19/2020 06:32:20New subject after splitting Last edited by: Jen_Moderator at: 08/19/2020 06:55:32Removed E-Mail address. |
|
8/19/2020 11:38 AM | |
Joined: 5/8/2017 Last visit: 9/30/2024 Posts: 13 Rating: (0) |
Good Day. USB adapter A2 specification. SIMATIC S7 Type :6GK1 571 0BA00 0AA0 May i know , means of MLFB number ? Thank You |
8/24/2020 7:48 AM | |
Joined: 5/8/2017 Last visit: 9/30/2024 Posts: 13 Rating: (0) |
Good Day. I am used X126 port at Sinamics DCM Drive . PG/PC setting used - USB.S7USB.1 Thank You |
8/25/2020 3:11 PM | |
Joined: 11/19/2019 Last visit: 10/2/2024 Posts: 10 Rating: (0) |
Timing is great, so I had a problem last week. The cable pc adapter usb (972-ocb20-0xa0) I used was connected to the dcm driver online, but it gave an error while uploading to pg. I replaced the connecting cable and the problem was resolved maybe the same problem. Just an idea |
8/26/2020 8:36 AM | |
Joined: 5/8/2017 Last visit: 9/30/2024 Posts: 13 Rating: (0) |
|
Last edited by: Satia at: 09/21/2020 11:45:57 |
|
8/27/2020 10:13 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (878) |
Please refer attached sheets (extracted from Siemens 6RA80 manual) which will help you to set paratemetrs & drive commissioning via Starter.
Attachment6RA80 commissioning with starter.pdf (712 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on