5/12/2016 9:09 AM | |
Joined: 8/5/2015 Last visit: 9/20/2021 Posts: 120 Rating:
|
hello i have pasic panel and have project on it and i wanna upload project from panel who know how it make? |
5/12/2016 9:40 AM | |
Joined: 5/28/2008 Last visit: 12/9/2023 Posts: 4486 Rating:
|
Hello, First check that you are using the correct cable: Which connector cables are available for connecting to SIMATIC Panels? And please note that if you take a backup, you won't be able to edit it if the programmer didn't downloaded the project to the panel with option "Back Transfer" How do you back transfer the projects of an operator panel and what should you watch out for? If you need only to take a backup (an image file) (i.e. non editable), then see the following links: |
Ayman Elotaify |
|
This contribution was helpful to
4 thankful Users |
Follow us on