3/29/2016 5:43 PM | |
Joined: 3/22/2016 Last visit: 3/29/2021 Posts: 2 Rating:
|
Compatibility check : Hi Is anyone able to help me check if the following items are compatible. We do not get any fiber link between the switches. Fiber cable is 350m and is tested with Fluke DTX We use the following parts in the network: fiber cable: http://www.nexans.be/eservice/DirectToProduct.nx?CZ=Belgium&language=nl&OID=540187367 6GK5308-2GG00-2AA2 Switch 6GK5004-1GL00-1AB2 Unmanaged switch 6XV1843-5EH10-0CA0 Patch cord 6GK5992-2AL00-8AA0 Media Module Switch -> Media module -> patch cord -> fiber -> patch cord-> Unmanaged switch No link established. |
Follow us on