Industry Online Support
Technical Forum
4/22/2009 3:46 PM | |
Joined: 9/27/2006 Last visit: 1/25/2025 Posts: 12331 Rating: (2702)
|
Hello Abyrne; I would think what you need is the Teleservicefunctions library. It is the modem-to-MPI interface used with Siemens PLCs for remote monitoring, programming SMS and data exchange. http://support.automation.siemens.com/WW/view/en/15220172 You will have to use a TS Adapter (there are various types, with different properties, some with integrated analogmodemsome with ISDN modem, some for direct connection through outside modem)as descibed in the manual above. I have attached an illustration from the same manual showing connection diagrams for an external modem working with Teleservice and a TS adapter. Hope this helps, Daniel Chartier. |
4/22/2009 4:11 PM | |
Joined: 11/26/2008 Last visit: 12/8/2023 Posts: 101 Rating: (4) |
Thanks Daniel, That was just what i was looking for! ~Aidan |
Follow us on