7/25/2011 2:14 AM | |
Joined: 10/7/2005 Last visit: 3/20/2025 Posts: 3042 Rating:
|
Hello Zer0 I don't have any hands on experience to offer for your choosen Adaptor, but say the description onebay is pretty clear when it states that: "1.) Double-click on "PC Adapter (MPI)" to set the parameters of COM port and MPI port. The adapter does not support "PC Adapter (PROFIBUS)" option" |
Cheers |
|
7/28/2011 4:09 PM | |
Joined: 6/15/2011 Last visit: 12/4/2024 Posts: 25 Rating:
|
Is it possible to use Ethernet cable to monitor/programm S7-300 instead of MPI cable? Thank you
|
7/28/2011 5:03 PM | |
Joined: 9/27/2006 Last visit: 3/21/2025 Posts: 12344 Rating:
|
Hello Zer0; Yes, it is possible (and easy)to download/monitor your PLC over Ethernet, if you have an Ethernet interface (CP 343-1, or Profinet interface on the CPU) setup and configured. There are many threads on the forum concerning this issue, such as this one: /tf/WW/en/Posts/24064 Hope this helps, Daniel Chartier |
Follow us on