1/13/2012 5:37 AM | |
Joined: 9/16/2008 Last visit: 2/20/2023 Posts: 56 Rating:
|
Hi, While try to installed the USB PC adapter V2.0 its not happening showing an Error V8.1 installed and V2.0 not able to installed over it. However in my system there is no sfotware with V8.1. Can anyone give some solution regarding this. I need to configure some device Profibus address using this adapter. Find attched the Error file and also the installed software. AttachmentUSB PC Adapter Error.zip (219 Downloads) |
1/16/2012 6:10 AM | |
Joined: 2/6/2009 Last visit: 3/10/2023 Posts: 932 Rating:
|
Hi, The information about the installation of the Set PG/PC interface in the attachment. Upgrade your PC to Windows XP SP3, that can also cause problem some times. AttachmentHow to install the set PGPC driver.pdf (292 Downloads) |
_______________________________________________________________ |
|
1/16/2012 6:18 PM | |
Posts: 947 Rating:
|
for step 7 5.4sp5 and windows xp sp2 I download software from support and also make update Firmware |
Follow us on