12/14/2018 10:00 AM | |
Joined: 1/17/2018 Last visit: 12/3/2024 Posts: 24 Rating: (2) |
I have the same task, but something extra:I also have PN IO system. My idea was to use 2 onboard PN connectors for the PNIO ring, and the remaining 2 PN connectors for the DCS modbus communication. But I got a request to poll 5 slaves. With DCS+PN IO system all my PN connectors are used up already, do I need CP 443-1 for polling the slaves or can it be done with a switch? Sample connection scheme would be very appreciated... ------------ Edit Or, something to convert Modbus <-> Profibus? And I can use the intergrated Profibus connectors? ----------- I was thinking this hardware config ------------------------------------------------------------------------------------------ |
Last edited by: Adcsi at: 12/14/2018 10:39:09 AMLast edited by: Jen_Moderator at: 12/14/2018 12:23:11 PMNew subject after splitting Last edited by: Adcsi at: 12/14/2018 1:17:48 PM |
|
12/14/2018 4:01 PM | |
Joined: 1/17/2018 Last visit: 12/3/2024 Posts: 24 Rating: (2) |
Hi, The 5 additional devices which came into consideration in a late point of time, are on modbus tcp protocol. |
12/14/2018 5:56 PM | |
Posts: 3093 Rating: (323)
|
Then it is still the question: are the servers capable to hold two ModbusTCP connections simultaneously? |
12/14/2018 6:07 PM | |
Joined: 1/17/2018 Last visit: 12/3/2024 Posts: 24 Rating: (2) |
No, they are not. But that is not needed and not planned. |
Follow us on