7/4/2013 8:44 AM | |
Posts: 39 Rating:
|
Hiii, What is the use of OLM and Repeater? |
This contribution was helpful to
1 thankful Users |
7/4/2013 8:49 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
What should you watch out for when using the RS485 repeater in PROFIBUS and MPI bus systems?in case of copper cable. In case of FO cable - is using OLM device. (The PROFIBUS OLMs are designed for use in optical PROFIBUS field bus networks. They enable the conversion of electrical PROFIBUS interfaces (RS485) into optical PROFIBUS interfaces and vice versa.) best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
7/4/2013 9:13 AM | |
Posts: 39 Rating:
|
Dear, Which one is better for long distance communication? |
7/4/2013 9:15 AM | |
Posts: 153 Rating:
|
FO is better but costly..... More info on OLM hera : OLMs? |
Follow us on