1/29/2021 11:57 AM | |
Joined: 1/4/2021 Last visit: 1/25/2023 Posts: 2 Rating:
|
Hi all, Im looking to use two push buttons (On and Off) on the HMI, no physical/hard wired On/Off. Both start in an Off state (Pushbutton_Square_G_Off_256c & Pushbutton_Square_R_Off_256c), when ON is selected (Pushbutton_Square_G_On_256c), on the HMI I want this to Set Bit in the program but also activates the Off button (Pushbutton_Square_R_On_256c) so then, when OFF is selected, resets the bit and deactivates the ON Button (Pushbutton_Square_G_Off_256c). Hope this makes sense and you can offer some help. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/29/2021 13:53:14New subject after splitting Last edited by: SteveGGG at: 01/29/2021 15:37:18 |
|
Follow us on