1/26/2023 10:02 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello AVERF you do not know the runtime loader? So how do you work on the WICC Runtime Advanced System? Its a little program that you can start manually or start in autostart. Its quite the same loader as on the Panels. If you are in transfer mode you can load directly from Engineering Station. If you work without RT Loader then you have to do the transfer manually. In this case check if you have all needed files: https://support.industry.siemens.com/cs/de/en/view/109740696 (-> last entry) Check if you copy the generated *.pwx file to get all the user information. overwrite in the Runtime folder and then start the Runtime. This will import automatially the user administration informations and everything should work if you have programmed it correctly. If it works in Simulation and not on RT system then its definitive these issue. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on