Industry Online Support
Technical Forum
2/18/2010 9:55 AM | |
Joined: 8/10/2005 Last visit: 2/7/2022 Posts: 3609 Rating:
|
Import of a Technical Question of an User Wadzanai wrote: I have a touch panel (MP377) and i have three user levels i.e. level0, level1 and level2. Level0 having the least privileges. I would want to automatically log in a level0 user when either the level1 or level2 user logs out. Please help, my client urgently needs an answer. Wadzanai |
2/23/2010 5:39 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, you can do following: Use the "Scheduler" -> and there the event "change user" and as parameter "GetGroupNumber". In the tag, there you can readwhich user group are log on. Furthermore: In the PLC you can evaluation this tag. After then you can setwith the "job mailbox"a "define" user with the area pointer number "23". -> see the communcation manual http://support.automation.siemens.com/WW/view/en/18797552 (Look to chapter 2.4.1.7) Thats all. regards, |
Follow us on