2/22/2024 7:10 AM | |
Joined: 1/21/2013 Last visit: 4/17/2025 Posts: 3764 Rating:
|
Hi mdarende, Restrictions on user management depend on how you manage users (locally or centrally). WinCC Unified PC Runtime V17 allows up to 200 users, but if you use Central User Management (UMC), only 10 users can be used without an additional license. To be honest, I have never used UMC, but according to the UMC Web User Interface Manual (Chapter 8), you have to admit that you owe the required licenses. Kind regards |
Follow us on