5/27/2010 12:45 PM | |
Joined: 9/23/2005 Last visit: 3/14/2025 Posts: 4406 Rating:
|
Hi, witch time interval has this cyclic OB? |
Denilson Pegaia |
|
5/27/2010 1:27 PM | |
Posts: 65 Rating:
|
I tried to set up various intervals. But I there is no positive result In attachment is an example of my program. PID_Compact is working always now, I found a little error in project. But I still can't read or write data by master device (PLC is slave), when I use PID_Compact in my project. Which time intervals must be optimal in my case? AttachmentSGU.zip (960 Downloads) |
6/2/2010 5:54 PM | |
Joined: 9/23/2005 Last visit: 3/14/2025 Posts: 4406 Rating:
|
One Idea is to monitor the Status not with the condition status <> 0 but else with error = true. I don't have hw to mount examples at this moment... However I have a sample that has alread worked and uses Modbus. The coments are in portuguese, however the main topics are language independents. AttachmentChapa1.zip (934 Downloads) |
Denilson Pegaia |
|
6/3/2010 12:34 AM | |
Posts: 65 Rating:
|
Thank you! I'll try it! |
Follow us on