5/29/2014 3:44 PM | |
Joined: 4/3/2014 Last visit: 9/9/2022 Posts: 54 Rating:
|
Thanks sir for answering Can you give more information about how we send and recieve data ? Best regards Ali ALKARN
|
5/29/2014 3:48 PM | |
Joined: 3/21/2006 Last visit: 12/18/2022 Posts: 10221 Rating:
|
Herehttp://support.automation.siemens.com/WW/view/en/25166781from Siemens point of view. |
5/29/2014 7:35 PM | |
Joined: 11/21/2007 Last visit: 1/21/2023 Posts: 2321 Rating:
|
Here is the Link for Downloading the Profibus GSD File for all SINAMICS Drives ( CU320 GSD shall be in SINAMICS S120 ) : Link The following link gives a lot of information regarding Controlling SINAMICS S120 in Profibus / Profinet : SINAMICS S: Speed control of a S120 with S7-300/400 (STEP 7 V5) via PROFINET/PROFIBUS Although this covers Control using SIMATIC-S7 , but would provide a nice glimpse into the way it works. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
5/30/2014 10:39 AM | |
Joined: 4/3/2014 Last visit: 9/9/2022 Posts: 54 Rating:
|
Thank you all that was usefull information |
Follow us on