5/19/2014 3:03 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Dear N. Vijay There is no other controller !!! The 25A SINAMICS DCM has been adapted to fire a set external FIeld Control Thyristors and and a large External Armature control Stack. I must say, this is quite innovative BUT AGAINST ALL NORMS AND RECOMMENDATIONS !! I understand that there are many such installation ( All supplied from China ) Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on