12/10/2014 5:29 PM | |
Joined: 3/30/2010 Last visit: 3/23/2022 Posts: 43 Rating:
|
If I open a V11 project in TIA V11, then I can see the complete cross reference list for the tag.But if I open this same project in V12, the cross reference dont show thetag usein the HMI anymore.... Ask1) How is that possible?? Is this functionality dissapeared from V12 (and V13)? And now i'm talking about cross reference....i remember some "old" but very usefull options... Ask 2) Is it possible to select cross reference from the tag adress, without searching the tag in theprogram code of in the tag list? (but just by typing the tag, this was possible in S7V5) Ask 3) Is it possible to see overlapping memory area's in the cross reference? (this was possible in S7V5)
|
Last edited by: Min_Moderator at: 12/11/2014 12:18 PMSplitted |
|
Follow us on