6/13/2017 10:21 AM | |
Joined: 6/26/2013 Last visit: 10/19/2024 Posts: 143 Rating:
|
Hello John,
You can find basics on screen navigation in the following link. You will have to set navigation at every screen. Basics on screen navigation (Basic Panels, Panels, Comfort Panels, RT Advanced) For creating a delay before activating another screen, you need to do some scripting. Take a look at the following FAQ about how to create a delay in HMI. How do you implement a wait function (delay) in a Visual Basic script in WinCC flexible? You can use the script provided in above link to activate screen via some internal tag after the delay. You call your script in the Click event of your button. For further information on scripting and its use in WinCC TIA, please visit the following link: Working with user-defined VB functions (Panels, Comfort Panels, RT Advanced) There is also a Demo Project available for WinCC Advanced V13 at the following link: Demo project for WinCC Runtime Professional V13 SP1 If it helps, please rate. Regards. |
meeda_ |
|
Follow us on