10/9/2016 5:53 PM | |
Joined: 9/23/2005 Last visit: 4/21/2025 Posts: 4406 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: in this simple sample, controller FB variables are automatically created on HMI tag table, following the controller's folders (group) structures. Requirements: TIA V14 SiVArc Project with a minimum configuration: S7-1500 configuration, Configuration main steps:
Result: on HMI → HMI tags a new group (folder) was created (Group_1, like as the controller) and, inside,a “Group_1_Data_block_1” tag table was created with the related controller instance DB variables (Data_Block_1_off, Data_Block_1_on, Data_Block_1_Status) References: TIA Portal online help: Help → Show help contends → SIMATIC Visualization Architect Project: Due a size/ format restrictions, the projects (one before and one after SiVArc generation) were first archived as zap14 format and after that attached to a zip archive (.zip). Attachmentprojects.zip (319 Downloads) |
Denilson Pegaia |
|
5/18/2018 2:13 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by AutoGen_631738 is split to a separate thread with the subject How can create a rule for tags in global DB and connect with faceplates?. Best regards |
Follow us on