10/9/2016 5:45 PM | |
Joined: 9/23/2005 Last visit: 4/21/2025 Posts: 4406 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: in this simple sample, controller FB variables are automatically created on HMI tag table. Requirements: TIA V14 SiVArc (SIMATIC Visualization Architect) Project with a minimum configuration: S7-1500 configuration, Configuration main steps:
Result: on HMI → HMI tags a “Data_block_1” tag table was created with the related controller instance DB variables (Data_Block_1_on, Data_Block_1_Status) References: TIA Portal online help: Help → Show help contends → SIMATIC Visualization Architect Project: Due a size/ format restrictions, the projects (one before and one after SiVArc generation) were first archived as zap14 format and after that attached to a zip archive (.zip). AttachmentProjects.zip (207 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on