10/9/2016 6:11 PM | |
Joined: 9/23/2005 Last visit: 4/21/2025 Posts: 4406 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: in this simple sample, one HMI screen is copied from the project library to the HMI project following the controller FB properties. Requirements: TIA V14 SiVArc Project with a minimum configuration: S7-1500 configuration, Configuration main steps:
Result: The FB Block_1 (instance DB FB_Block_1_DB) inputs and outputs are configured as HMI tags, a screen MyHMIScreen is added to HMI screens, on HMI MyHMIScreen one MyHMIFaceplate_1 is copied, with name Block_1_DB, the intern text field is renamed to “Block_1_DB”, the IO field variable is connect to Block_1_DB.Status PLC tag, the Button is connect by invert bit function to the Block_1_DB.On PLC tag. References: TIA Portal online help: Help → Show help contends → SIMATIC Visualization Architect Project: Due a size/ format restrictions, the projects (one before and one after SiVArc generation) were first archived as zap14 format and after that attached to a zip archive (.zip). AttachmentProjects.zip (605 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
3 thankful Users |
9/6/2017 11:38 AM | |
Posts: 4 Rating:
|
Hello DS, I can send you working example with faceplate in popup screen. Best regards |
9/8/2018 7:40 AM | |
Joined: 7/4/2015 Last visit: 4/22/2025 Posts: 4 Rating:
|
Can u plz Share the Sample Project of SiVArc with the use of POP UP screens for faceplates. |
Follow us on