12/30/2017 1:23 PM | |
Joined: 9/23/2005 Last visit: 4/4/2025 Posts: 4406 Rating:
|
Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: In this simple sample, controller FB variables are automatically created on HMI tag table and alarms will be created based on these variables. The variable creation was already detailed on Topic “V14 – Simple Sample: SiVArc – creating Tags on HMI” (https://support.industry.siemens.com/tf/us/en/posts/v14-simple-sample-sivarc-creating-tags-on-hmi/156032/?page=0&pageSize=10). I copied this description here and add the steps related to alarms in “Alarm specific steps” division Requirements: TIA V15 SiVArc (SIMATIC Visualization Architect) Project with a minimum configuration: S7-1500 configuration; HMI (or WinCC Professional) Configuration main steps:
Alarm Specific steps: (STEP 1 the alarm definition should be place on Project Library master copies - to do it an alarm should be created on HMI and copied to library):
(STEP 2 copy the alarm definition to the project library)
(STEP3 Ceate SiVArc rules):
Result: On HMI → HMI tags a “Data_block_1” tag table was created with the related controller instance DB variables (Data_Block_1_on, Data_Block_1_Status) On HMI → HMI Alarms → Discrete Alarm a Discrete_alarm_1 will be created with the Text = “Alarm at Block_1_DB” and with trigger tag = “Block_1_DB_Status” References: TIA Portal online help: Help → Show help contends → SIMATIC Visualization Architect Project: Due a size/ format restrictions, the projects (one before and one after SiVArc generation) were first archived as zap15 format and after that attached to a zip archive (.zip). Attachmentproject.zip (517 Downloads) |
Last edited by: Denilson Pegaia at: 12/30/2017 1:24:27 PMDenilson Pegaia |
|
This contribution was helpful to
3 thankful Users |
11/24/2020 10:24 AM | |
Joined: 2/9/2015 Last visit: 12/9/2024 Posts: 11 Rating:
|
Hi, If I don't set Trigger bit value in Plus-ins, the trigger bit of generated alarms will all be 0. |
Follow us on