2/10/2021 12:45 PM | |
Joined: 12/16/2016 Last visit: 1/6/2025 Posts: 13 Rating:
|
I cannot download to a KTP400 Basic PN with TIA V16 due to missing panel image. # I've attempted to downloaded the images from the zipped folders mentioned previously including the Basic Gen 2 panel one which I think should contain the image for this HMI. I copied these I think into the correct folders manually. This worked for my TP1200 comfort panel and got rid of the same error I was getting with that one. The tech support told me to download DVD3 which I have and installed using the .exe file. First for just the new HMIs 2.5GB and then when that didn't work selected the full image library including all the legacy HMIs and conversion images required for upgrading etc (8-9Gb) and this still hasn't put the image file in the right place for the KTP400 basic PN. Now checking to see if there are any updates I'm missing. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/27/2023 13:56:09New subject after splitting Last edited by: Jen_Moderator at: 11/29/2023 07:14:21Headline optimized. |
|
Follow us on