11/21/2022 11:33 AM | |
Joined: 2/17/2020 Last visit: 1/17/2025 Posts: 1167 Rating: (214) |
Hi Vinizuca, Numerous improvements have been developed for WinCC Unified V16 with the Updates released (and even more for V17...). Please try to upgrade to the latest WinCC Unified V16 Update via this link, and then make sure you only give the project user the highest (Administrator) permission, not all of them. Also, make sure that the PLC is not protected against HMI access and that, in the case of IO fields, the format is Input/Output. |
A rating will be well appreciated. |
|
Follow us on