5/5/2023 1:50 PM | |
Joined: 4/27/2015 Last visit: 12/19/2024 Posts: 11 Rating:
|
I have this problem too. TIA 18 S7-1200 and KTP900. I just get empty space where the event text should be on the HMI in diagnostic buffer view. It's visible in the PLC diagnostic buffer. Normal system messages from the PLC show fine in HMI diagnostic buffer view. I have only one language enabled which is English (United Kingdom) and all languages of the device display / web server are set to English (United Kingdom). The previously suggested fix seems unrelated. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/08/2023 07:11:09New subject after splitting |
|
5/12/2023 7:43 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello BenjaminIT do you use also the English(UK) as Runtime Language in the HMI? this has to fit to the settings in the PLC. Which FW Version do you use on PLC and which Image version on HMI? I would try a: https://support.industry.siemens.com/cs/de/en/view/109778709 Then try again. Do you have the same issue in Simulation of the HMI? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on