10/16/2023 10:21 AM | |
Joined: 6/26/2023 Last visit: 10/31/2023 Posts: 3 Rating:
|
Currently, I'm working with WinCC Unified V18 and facing an issue related to screen resolution and scaling. I have an MTP700 UNIFIED CONFORT HMI with a resolution of 480x800 and a SIMATIC UNIFIED PC STATION with a resolution of 768x1024, where the server is hosted, and I can access it through the HMI. However, the screens have different resolutions and are not proportional. As a result, when I view the PC on the HMI, the screen isn't completely filled, and manual zoom adjustments are insufficient due to the differing scales. I would like to know if WinCC Unified has a built-in automatic scaling feature that can adjust the size and position of objects on the screen to match the resolution of the device where the project is being displayed. Is there a way to enable automatic scaling or a similar functionality to ensure that my project is displayed correctly on screens with varying resolutions, without manual adjustments? If such a feature exists, could you provide guidance on how to use it effectively? If such a feature doesn't exist in WinCC Unified, could you suggest best practices or alternative solutions for designing projects that adapt well to different screen resolutions? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/17/2023 07:42:22New subject after splitting |
|
10/16/2023 10:44 AM | |
Joined: 12/14/2022 Last visit: 10/27/2023 Posts: 46 Rating:
|
Hi @AutoGen_605389, you can do what you want on SIMATIC Runtime Manager, select the project you want (it must be stopped), click the gear symbol (Settings) and check the box at Autoscale - Adapt screen to window. |
igorcoraine.github.io |
|
10/16/2023 12:09 PM | |
Joined: 6/26/2023 Last visit: 10/31/2023 Posts: 3 Rating:
|
Hi, The PC runtime has the correct dimensions, the MTP700 accesses the PC through a web control window and in the HMI I can't fill the entire screen. I applied this runtime option but it didn't work |
10/17/2023 10:36 AM | |
Joined: 12/14/2022 Last visit: 10/27/2023 Posts: 46 Rating:
|
It doesn't work only on the HMI or anywhere? |
igorcoraine.github.io |
|
Follow us on