3/6/2025 7:45 PM | |
Joined: 12/11/2024 Last visit: 4/23/2025 Posts: 5 Rating:
|
Hello, I'm running into an odd inconsistency with the texts between my local simulated HMI and my loaded HMI on a remote station. Some things I've tried with no change are making sure that my screen resolutions are the same, using unified version 3 on both stations, making sure that my pixels are consistent between pages, and making sure text is centered. This is an odd situation because the shifting text is inconsistent. One text may be in the correct position and after I switch off that screen and come back, that same text would be shifted. I've had this issue regardless of where the text lives whether it'll be in a window, a faceplate, or neither. I've attached a folder with a few examples, local is what I have simulated and remote is what has been loaded. Please let me know if you have also ran into this issue and if you have found any workable solutions. Thank you! Lisa Attachment00 - HMI screenshots.zip (25 Downloads) |
3/11/2025 3:02 PM | |
Joined: 11/13/2018 Last visit: 4/25/2025 Posts: 90 Rating:
|
Hello AutoGen_5707642, I recently encountered an issue that seems to be affecting others as well. Here’s how I resolved it:
Hope this helps! Let me know if you have any questions or need further clarification. AttachmentUnifiedRT_05.00.00.30_Patch_01.zip (23 Downloads) |
Last edited by: Moderator_Lan at: 03/11/2025 15:13:47links optimized Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on