2/19/2016 8:17 AM | |
Posts: 6 Rating: (0) |
Here is my input connections. Brown colour is +24V and blue colour is negative. I think is correct. |
2/19/2016 8:30 AM | |
Posts: 1529 Rating: (202) |
Maybe the camera angle, but it looks like you are one pin off on all of your connections. X10:1M should be brown (+24V). |
2/19/2016 9:20 AM | |
Posts: 1529 Rating: (202) |
Is the right wire connected? With the 50 wires in the silly cable, it is sometimes difficult to read the tag properly. |
2/19/2016 9:30 AM | |
Posts: 6 Rating: (0) |
Yes, here is a pic with that. I revised all the pin numbers to be like in the wiring of Siemens example. |
2/19/2016 10:11 AM | |
Posts: 1529 Rating: (202) |
No idea then, all of mine work fine. Are you getting an alarm after you enable the SON? |