5/2/2018 2:42 PM | |
Joined: 10/11/2006 Last visit: 1/22/2025 Posts: 5985 Rating: (824)
|
Hello, do you have a V90 Standard or Profinet Version (V90PN)? The Profinet Version has the basic positioner (called EPOS). This can be used, and on the PLC side you can take the SINA_POS block from the Drive Library. Here is one example: https://support.industry.siemens.com/cs/ww/en/view/109747750 Technology object would also be possible. Here also one example: https://support.industry.siemens.com/cs/ww/en/view/109743917 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on