3/16/2019 8:02 AM | |
Joined: 4/28/2015 Last visit: 8/17/2024 Posts: 1 Rating: (0) |
I am facing following problem in siemens v90 drive positioning control: i am using motor: SIMOTICS S-1FL6042-1AF61-0LA1 Encoder: ABS.MT.20-bit 1. Currently i am using SINAPOS block for position control and homing teaching is done by drive keypad. 2. i am using profinet telegram 111 for communication with my 1217 PLC. 3. The problem I am facing right now is the disturbance in homing position on Power on and off the system or after restarting the system. 4. It takes any random negative value as its actual position. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/18/2019 11:36:55 AMNew subject after splitting |
|
Follow us on