8/10/2016 10:43 AM | |
Joined: 7/22/2011 Last visit: 12/23/2023 Posts: 78 Rating: (2) |
Does exist a way to read via Profinet the read the drive rxxxx parameters ? Yours Sincerely, Pier Giovanni |
8/10/2016 11:37 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hello, where you get ""format 0x44" output."? Can you provide a screen?
Christoph |
8/10/2016 3:21 PM | |
Joined: 7/22/2011 Last visit: 12/23/2023 Posts: 78 Rating: (2) |
Hi, I have only one drive. Here is the test with all informations from block. Yours Sincerely, Pier Giovanni |
8/11/2016 9:55 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hi, use axisNo = 2 please! Regards Christoph |
8/11/2016 12:09 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hello, telegram 1 and axisno=2 works without any problem here. Regards Christoph |
8/11/2016 1:30 PM | |
Joined: 7/22/2011 Last visit: 12/23/2023 Posts: 78 Rating: (2) |
Hello, so, is the HW-id is to be used as parameter axis number for the SINA_PARA block ? Regards, Pier Giovanni |
7/30/2018 11:49 AM | |
Joined: 6/12/2018 Last visit: 8/3/2023 Posts: 4 Rating: (0) |
can you send me the exact produre to do that |
7/30/2018 9:12 PM | |
Joined: 7/22/2011 Last visit: 12/23/2023 Posts: 78 Rating: (2) |
Hello, here my test project; lokk to seg. 10 Pier Giovanni AttachmentControlloAssePosizone (FB1).pdf (162 Downloads) |
This contribution was helpful to1 thankful Users |