4/16/2022 6:19 AM | |
Joined: 4/15/2022 Last visit: 5/24/2022 Posts: 15 Rating:
|
One more question, can I use the value of analog value (LWE) in an arithmetic instruction (soft comfort)? |
4/16/2022 6:41 AM | |
Joined: 12/18/2014 Last visit: 12/3/2023 Posts: 31538 Rating:
|
But note: The addresses in the VM area are byte oriented. The addresses are 0 - 850 for user. Bit eg. V0.0 = byte address. bit address. Byte e.g. VB0. VB0 included the bits V0.0 -V0.7. Word eg. VW0. VW0 included VB0 and VB1. Also V0.0 - V1.7. AttachmentLOGO! Bit, Byte, Word and DWord.pdf (352 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on