11/4/2015 12:06 PM | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 11/9/2008 Last visit: 8/23/2024 Posts: 410 Rating: (6) |
Hi All, I need some software development help for Water Plant. I have Valve sequence. Please see below table
From above table take e.g. of Air Release – 1. 2 Min is running time set point. 2. If Air release start it will check Priority number to open / close the valve then Time delay (X Seconds) for opening or closing of valve and Open valve / Close valve. 3. I need to develop this logic as per above table selection. Priority, Time and Opening and Closing of Valve will changeable. 4. I don’t want use too many timer because I have another Sequence it has almost 24 steps same as above. 5. Please guide me proper way to develop this logic.
Regards, Yogendra G
AttachmentValve sequence.pdf (293 Downloads) |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: YogendraG at: 11/4/2015 12:08:40 PMPlease find the attached Valve sequence Documents |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Follow us on