7/12/2017 3:54 PM | |
Joined: 10/11/2006 Last visit: 7/1/2022 Posts: 5225 Rating:
|
Hello, using SINAMICS S120 Booksize System with common DC link, would provide some advantages like a common infeed and optional regenerative feedback, a common braking unit and resistor (e.g. used in case of line fault when having a regenerative infeed module). Functionality for winder and positioning can be included in the drive software using DCC (Drive Control Chart). Some of the functionality is available as application example: https://www.automation.siemens.com/mc-app/sinamics-application-examples/Home/Index?language=en Using SINAMICS G120 would also provide the required things like profinet interface, brake module, and brake resistors, option to diagnostic software. There each device has its own AC connection and needs also its own braking resistor (braking chopper is part of the device). I would recommend to contact you local Siemens representative to discuss the different possibilities in detail. |
With best regards, |
|
Follow us on