3/19/2021 2:26 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello Isaac; Are your errors linked to the VB script or to the connection to the Rockwell PLC? Which PLC model are you connecting to, what driver have you setup between the TP 1200 Comfor and the PLC? For a Controllogix or Compactlogix CPU you should use the Ethernet/IP driver available in WinCC, the first step is always to configure the connection properly and ensure there is an active communication channel; the second is to create variables in your script that the PLC accepts natively; are you sure the PLC accepts 4-byte registers (DINT) for its time setting? Can you give us a screenshot of the errors you are getting? See the WinCC v16 Engineering manual for more information o the drivers for Rockwell PLCs. https://support.industry.siemens.com/cs/ww/en/view/109773787/96523272203 Hope this helps, |
Last edited by: dchartier at: 03/19/2021 14:30:10 |
|
Follow us on