9/17/2014 1:34 PM | |
Posts: 17 Rating:
|
Hi Jens, I've added the project im working on at the moment, there you can disable diffrent parts of the script from the HMI so that part isn't written into the csv file. If i understand you correctly, that is what you need. The way that works is. If TagXX=true then Write ABC end if If TagYY=True Write DEF end if And by setting it up correcly, the csv file will either only show 1 of the texts, none or both. AttachmentUSB_Data_Script.zip (273 Downloads) |
Follow us on