4/26/2016 10:28 AM | |
Joined: 2/6/2015 Last visit: 9/21/2017 Posts: 38 Rating:
|
HMI : TP1500 - Wincc Adv. Comfort PLC : S71500 TIA Portal - V13 SP1 UPD8 Hi All, I have a problem again with the VB Script while referring to a PLC UDT Variable. A reference to the PLC Variable already existed in the project and I just added one more variable to this PLC UDT variable and from then on, I get this error with the vb script that it cannot find this new variable. In the warnings, there is an unwanted 0 in the variable and I dont know how to remove that. Anyone had this problem and know how to remove this? The problem variable, I have pointed it out with arrows. Thanks and Regards, AttachmentVBSPlcUDt.docx (311 Downloads) |
Follow us on