5/8/2019 9:28 PM | |
Posts: 6 Rating:
|
Hi, I have similar problem i use the ATC-2000 converter without the Modbus RTU>TCP translation. Now I try to find the solution like Vcom on S7-1200. it is possible to get from you the code? EDIT: More explanation: I would like to use ATC-2000 (serial to Ethernet converter) to establish communication between S7-1212 and Zamel RXM-01 (home automation Modbus<->"exta free" translator) the simplest way will be to buy Modbus getaway or CM1241 but its cost. One of my ideas is to calculate frame by the Modbus_master block from lib. and copy from the temp and after that paste to temp in MB_Client. It is possible or maybe you have another solution. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/09/2019 11:17:34New subject after splitting Last edited by: eldzii at: 05/09/2019 13:11:15 |
|
Follow us on