7/13/2016 6:44 AM | |
Joined: 9/14/2012 Last visit: 1/11/2023 Posts: 77 Rating:
|
Dear Zaho, Thanks for your reply.Now i understood the Velocity setpoint concept clearly . But now i have one issue,my motor speed not increased more than 670 Rpm. Example If i gave speedsetpoint = 1200000LU/min. My motot runs in 670 RPM ALSO IF i gave Speed Setpoint= 5000000LU/Min .Also My Motor Runs In 670 RPM Only I thing Some Factors limited My Velocity. Also I Checked My Maximum Velocity In Limits that is 300000 1000lu/MIN Here With I attached my Starter Backup Kindly Any One Help Me...... AttachmentFeeder_d.zip (45 Downloads) |
Follow us on