3/7/2018 8:34 AM | |
Joined: 4/24/2006 Last visit: 4/24/2025 Posts: 8965 Rating:
|
Hello, Does the HMI panel KTP400 Basic contains a Sm@rtserver license? Perhaps this link might help: Remote Access to SIMATIC HMI Control Panels Best regards, Wizard |
Last edited by: Wizard at: 3/7/2018 8:35:27 AM |
|
This contribution was helpful to
1 thankful Users |
3/7/2018 9:37 AM | |
Posts: 102 Rating:
|
Thanks for the answer, Wizard, it seems like a possible solution.
Yes it does. It's active as well (already was when I first tried too), but using it seems to entangle installing another lil' helper that I theoretically shouldn't need. I was actually hoping to use the same method for the HMI as for the other components in the network: the already active VPN connection with the current setup by which I can access at least PLCs, Routers and PCs just fine, but which, with Sm@rtServer on as well as off it just doesn't seem to work with the HMI |
Follow us on