11/10/2017 9:56 PM | |
Joined: 12/2/2014 Last visit: 3/13/2025 Posts: 14 Rating:
|
Hi everybody. I follow the guide in the attached file to open a VPN Tunnel between two stations. In one side there is a S7-1500 CPU with a CP-1543-1 and one Siemens Router. In the other side there is a S7-1200 CPU with a CP-1243-7 LTE to connect in internet. The result is ok, so the VPN tunnel is correctly opened and the two stations are connected, but I can't communicate between them. If I insert a "PUT" instruction I have an error, because on the CP side i must use the public-static IP adress of the SIM card (172.18.51.xx) and in the other side I have the IP of CP-1500 (192.168.1.xx). There is somebody that know a system to exchange data between stations with different IP's? Because the GET/PUT istructions require the same IP address... Thanks AttachmentCONNESSIONE VPN_CP1243_CP1543_DOC_V10_en.pdf (82 Downloads) |
11/10/2017 9:58 PM | |
Joined: 12/2/2014 Last visit: 3/13/2025 Posts: 14 Rating:
|
Here the error with the PUT instruction |
Follow us on