4/30/2011 7:33 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, In my opinion You could give the mentionned IP address 10.100.2.14 to the external interface of a scalance S612. The scalance S612 would be used in routing mode, and the second interface of the Scalance S612 would be placed in the range 192.168.0.x., for instance 192.168.0.30 The CPU must refer to the address 192.168.0.30 as default gateway. Now you can create a VPN tunnel with a PC running the Softnet security client software. More details on how to prceed here: http://support.automation.siemens.com/WW/view/en/22056713 |
Best regards |
|
Follow us on