Industry Online Support
Technical Forum
5/9/2008 8:16 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi joedub, Yes, it's sounds like a working solution. Just keep in mind the bandwidth needed for your application and if that's suitable there is no problem at all. And yes it's webbased. You only need the Primary Setp Tool once to set teh IP-Address of the devices because they come without an IP-address if they are fresh! Download: Primary Setup Tool v3.2 |
Best regards, |
|
5/12/2008 3:30 PM | |
Posts: 9 Rating: (0) |
Thanks for the responses. This has been very helpful. Now I just want some hardware to work with. Thanks again. |
Follow us on