5/25/2021 6:35 AM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating:
|
Hi Davinator, I have the Kepware licensed, I have D435-2DP FW 4.3V. I want to access the data through OPC driver in the kepware. I have opened the web-server as I have access to it. Now the question is the OPC server as per manual says we have to edit cfg.xml file, "<ENDPOINTDESCRIPTION URL="X127:4840"/>" I have no clue as i am new to Simotion software dont know how to access the CF card either Now as of I can see that in the cfg.xml its defaulted to the x127 port (correct me if i am wrong) Can i directly use the IP assigned to the x127 port on the kepware to give it the following address for the server [I am considering that OPC server is alredy default configured to x127 profinet port and so i can directly use it w/o changing the cfg.xml file on CF card] "opc.tcp://169.254.11.22:4840" If not then how can get that cfg.xml file from the CF card? DO i need special siemens PG to read it ?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/25/2021 13:59:11New subject after splitting Thanks and Regards |
|
Follow us on