9/5/2020 7:41 PM | |
Joined: 12/15/2019 Last visit: 5/2/2024 Posts: 20 Rating: (1) |
Hello , I have the same request , I have a machine with 6 winder and i want to know the possition of the encoder o calculate the inicial diameter . I thin we can have at leat two solutions - Using the telegram 103 to know the position of the encoder or use the TO and configured like and position axis , and move on velocity my concern is the speed control eficiency because i have a small dancer on the middle ..... I dont know if it's affect .
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/07/2020 10:22:39New subject after splitting |
|
9/8/2020 1:05 PM | |
Joined: 10/11/2006 Last visit: 6/13/2024 Posts: 5860 Rating: (795)
|
Hello, use 102 or 105. It is possible to switch on " Non position-controlled" 6.3.4 Non position-controlled operation The closed loop position control of an axis can be switched off/switched with the following Motion Control instructions: ● MC_Power ● MC_MoveVelocity ● MC_MoveJog The non-position-controlled operation is displayed with <TO>.StatusWord.X28 (NonPositionControlled) = TRUE. https://support.industry.siemens.com/cs/ww/en/view/109749262 |
With best regards, |
|
This contribution was helpful to1 thankful Users |