2/28/2019 9:39 AM | |
Posts: 6 Rating:
|
Hello I have some problem with set PG/PC interfaces. I have computer with win 10, and on this comp i have vmware virtual system win 7 64. I installed step 7 pro sr1 and sp1, sp2, sp3, sp4 and hf11 on virtual machine. Computer don't have hardware com. I used conwerter usb to rs232. I tried two ways for connection virtual rs232 to virutal machine. First is in settings of virt. machine i remove port com, and after start machine i connected usb divice and in divice manager appeared vitual port com. Second way was that i add com port to virual machine and let use phisical port of nativ system. In nativ system i instaled converter and it apeared as com 3. Problem is that i dont have PCAdapter for eg. MPI or PROFIBUS or AUTO on my set PG/PC interfaces and i can't connect to PLC with MPI protocol. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/28/2019 3:20:40 PMNew subject after splitting |
|
2/28/2019 2:07 PM | |
Joined: 9/21/2012 Last visit: 3/23/2025 Posts: 4345 Rating:
|
RS232 is not compatible with MPI (RS485). |
2/28/2019 3:06 PM | |
Posts: 6 Rating:
|
Thats Why I need PCAdapter MPI(it is convertrer rs232 to MPI). But I can't use it because there is no such a option in setPG/PC interface window in step7 |
2/28/2019 3:13 PM | |
Joined: 9/21/2012 Last visit: 3/23/2025 Posts: 4345 Rating:
|
The Siemens PC Adapter is connected directly to USB, not a COM port. |
3/4/2019 3:13 PM | |
Posts: 6 Rating:
|
PCAdapter its 6es7 972-0ca21-0xa0. In attachment print screen with divice manager window. System its a bit complicated because its win7 64 as virtual system on win 10. Computer don't have hardware com thats why i want to use converter usb<->RS232. problem is that there is no option in setPG/PC interfaces "PCAdapter.MPI" |
Last edited by: majkel1 at: 3/4/2019 3:13:27 PM |
|
3/4/2019 3:19 PM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
Hello, the adapter is not released for 64bit operation system, so the driver not available! https://support.industry.siemens.com/cs/ww/en/view/10420976 Note on compatibility with Microsoft Windows 7 64-bit
Christoph |
Last edited by: ChristophD at: 3/4/2019 3:19:54 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on