Industry Online Support
Technical Forum
6/12/2014 4:46 PM | |
Posts: 33 Rating: (0) |
Yes, it will work if there are more than one pulse within a second. in this case, distance between pulses can be bigger than 5 seconds |
6/12/2014 5:13 PM | |
Posts: 88 Rating: (12) |
My idea is to calculate the time between each pulse. After we can say for example 2L in 5s => 0.4L/s and doing that continuously... Is it a good way? |
Follow us on