Industry Online Support
Technical Forum
9/15/2007 11:24 AM | |
Posts: 7 Rating: (0) |
I have installed wcc 6.2 on two different computer with the same result. the first computer is a laptop with 512 MB ram, the secon a fixed station with 1,5 Gb ram, both computer with windows XP. I have made attempt of start runtime with two different project. - a converted old wcc project from version 5.1 sp1 - a test program with only two page with two button that switch between page e one button for exit WCC the result is the same, the runtime after a PC power on and after a first start of wcc explorer start. I turn of the project and from the second start of runtime the project don't work more. I have tryed with firewall on and off, and with antivirus off and on but the result is the same on both computer and with the two project. I send also a diagnose directory for 3 PC power on, the second PC power on give a unusual resul an unexpected error. Is theresame person that have the same problem ? How can I solve this problem ? Bye AttachmentDiagnose dir.zip (91 Downloads) |
9/17/2007 1:36 PM | |
Posts: 17 Rating: (2) |
HI Duffy_artur , I had similar problem. It was realted to the Dual core processor of PC. Have you installed this patch for WinCC. It has relaxed my life... http://support.automation.siemens.com/WW/view/en/25869221 Hope itwill work for you 2 . regards nitin |
Follow us on