2/26/2024 1:56 PM | |
Joined: 5/30/2023 Last visit: 4/16/2025 Posts: 4 Rating:
|
Hi Denilson, I am using WCCURT V18Upd 3, authentication is made through UMC, which itslef is linked to the AD of the company. I need to let some groups of operators access certain areas/functions, and block unthorized users. I tried adding custom roles to groups in the UMC webUI, but they do not reach the TIAPortal project : The groups get correctly in the TIA Portal, but the roles do not. Then I tried to create custom roles in the TIAPortal, and attach them to groups, but those roles do not get to the RT. when I use the function GetRolesFromUser() I only get "HMI Administrator, HMI Operator, HMI Monitor, HMI Monitor Client" Since I cannot ( I think ) get the group the user is part of, I am failing to understand how to implement a proper authorization method for the various users/functions Would you have an idea of how to get there ? Thanks in advance, Best regards, Thibault
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/27/2024 10:44:42New subject after splitting |
|
Follow us on