8/25/2009 11:04 AM | |
Joined: 7/17/2008 Last visit: 10/25/2013 Posts: 34 Rating: (2) |
Hey Jim, First of all you cannotuse WDS and iPDF at the same time in the same interface. Secondly if you buy a 788-2 take in account that only oneofits two interfaces could be configured with iPCF at the same time!!!! If you don't use "direct keys" in HMI, actually the HMI doesn't use Profinet, uses standard TCP/IP comm for his S7 links. If you use the L2T (layer 2 tunnel) in the Scalance W clientthat Eric metioned, you can connect up to 8 nodes to the client. Please read this FAQ: http://support.automation.siemens.com/WW/view/en/26562314 Some scenarios: http://support.automation.siemens.com/WW/view/en/31938420 Wich profinet update time do you need? Hope this info helps, anyway post any comment or doubt Regards |
8/26/2009 1:17 AM | |
Posts: 3 Rating: (0) |
Thanks, I'm starting to put this together. I'm still struggling with what my limitations are for incorporating the HMI. I've heardcommunications isslowed significantly when hanging an HMI off the same W747RR client module as the ET200S node, using iPCF.If I use a W788-2RR access point with one channel allocated to iPCF and the other not, would that intern require two seperate W747RR client modules? Onededicated for the ET200S node, and the other for the HMI. I'm trying toincorporate an HMI into the scheme using the fewest amount of hardware, yet maintainI/Othroughput times to no more than 100ms. I found the site below, under the "Profinet I/O" section, which allows one to configure a wireless based system and incorporate an HMI into the scheme. Unfortunately for me, it never places the HMI on the client side. Always on the AP side. I like the tool and it has me believing I can meet the time requirements I'm looking for but I still dont understand some of the results it displays. Please share if you know how to read the performance data results. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=25209605&caller=view Thank you for your help thus far, It's been very informative. Jim |
8/26/2009 9:55 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi Jim, Normally PN IO should not be effected by the traffic generated by the Panel due to the priority mechanism in iPCF. This ensures that PN IO frames are handled with a higher priority then the 'normal' frames. the only thing you should think about is the speed and the number of traffic you want to send but if it's a SCADA for monitoring only this won't be a problem at all. Just use a Scalance W788-1RR or a Scalance W784-1RR and as a Client you could use a Scalance W747-1RR or Scalance W747-1. You also write about an update of 100 ms maxcimum this would mean you want to have a PN IO Update time of 32 ms and 3 retries am I correct? This is no problem as long as your signal strength doesn't go below the 60% and you do need a channel which is free of interferences from other Wireless devices. In most cases this means that you should use 5 GHz frequencies. But check the Country Approvals for the Scalance W devices before you need to choose a channel since not every contry has the same regulations. Certificates for WLAN |
Last edited by: INS at: 8/26/2009 11:40 AMChanged the first part. Best regards, |
|
8/26/2009 2:35 PM | |
Posts: 3 Rating: (0) |
Excellent information guys, Thank you so much. |
Follow us on