2/8/2024 10:52 AM | |
Joined: 5/6/2022 Last visit: 4/22/2025 Posts: 587 Rating:
|
Hi aamirawan91, Based on what you say, from my point of view I would recommend the Unified PC option since I think it can give you much more versatility and meet your requirements more. In the end, with Unified you can use independent web clients, viewing it from any PC with any browser that is released like Chrome. For basic/comfort/advance, it would be for uses more than Sm@rtServer. I am attaching some links below to remote access that may be of interest to you so that you can evaluate: "Remote Access to SIMATIC HMI Operator Panels" "Remote access to WinCC Unified PC Runtime and Unified Comfort Panels" I hope I have been able to help you! Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on